10/25/2016 5:49 PM | |
Posts: 2 Rating: (0) |
what do i have tot do more i have installed my logo wit a cable to my network and network IP adress as 192.168.000.050 but when i run your program i do'n get connection with this IP . when i ping to the ip adress (off the logo) from my computer,i receive the packets can someone help my? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 10/26/2016 9:51:15 AMNew subject after splitting |
|
10/26/2016 10:32 PM | |
Posts: 3 Rating: (0) |
I can't connect to a logo either. |
10/26/2016 10:48 PM | |
Posts: 3 Rating: (0) |
Using windows 10 Logo! 230RCE Starts to connect, then says Logo & PC are not on the same subnet. Help |
10/26/2016 10:55 PM | |
Posts: 3 Rating: (0) |
Ethernet cable to Logo Logo IP 192.168.0.123 Subnet - 255.255.255.0 Gateway - 233.0.0.0 PC IP 169.254.142.102 Subnet - 255.255.0.0 Gateway - 0.0.0.0 |
Follow us on