10/27/2016 1:59 PM | |
Joined: 4/19/2016 Last visit: 10/3/2023 Posts: 25 Rating:
|
One question: Will be work Insigth v5 and a new PXC100D, PXC01D with firmware version 6 ? THX L.R. |
10/27/2016 2:56 PM | |
Joined: 6/4/2010 Last visit: 8/13/2024 Posts: 387 Rating:
|
Dear Lukas, You normally require the latest version of the Desigo Insight Management station for the latest controller firmware version. The exception is Desigo Insight V5.1Servicepack 2, with additional patch H47, which supports the Desigo PX V6.0 firmware. Please note that only the existing Desigo V5.1 firmware features are supported in this combination. There may be some limitations in the provided library as well. You can find the Desigo Insight V5.1 SP2, patch H47 under the following link: https://support.industry.siemens.com/cs/ww/en/view/109737999 (please contact your local Siemens sales office in case that you do not have access to the Extranet). Please note that we anyway recommend to upgrade Desigo Insight to V6.0. Desigo Insight V6.0 provides several advantages and improvements and ensures optimal system compatibility, reliability and performance. Best regards, Albis |
11/1/2016 1:28 PM | |
Joined: 4/19/2016 Last visit: 10/3/2023 Posts: 25 Rating:
|
.... unfortunately, upgrade licences from v5 to v6 is not so cheap. |
Follow us on