(0)| 10/13/2016 6:44 AM | |
|
Joined: 12/18/2014 Last visit: 1/21/2026 Posts: 36503 Rating:
|
There is also a delay with the LOGO!s series 0BA8. How long the time is depends strongly on the network and the cycle time. What time this is, I can not tell you. In the test between 2 LOGO! S with a minimum program, 0.05s were not safe. Times worked, then again not. Only from 0.1s onwards a secure transmission was ensured. As I said, only 2 LOGO!s and a minimum program. AttachmentProject.zip (276 Downloads) |
| 12/13/2016 3:59 PM | |
|
Posts: 4757 Rating:
|
New question published by jorgengyselinck is split to a separate thread with the subject Multiple logo's, can i use in every logo the maximum netwerk inputs/outputs?. Best regards |
Follow us on