5/2/2008 1:59 PM | |
Joined: 9/20/2006 Last visit: 3/5/2024 Posts: 307 Rating: (96) |
Dear hutdotedudotvn , MM420 units do not have braking chopper in it, so you cannot connect a braking resistor to it. This feature is available in MM440 only. If you do not connect a braking resistor depending on the amount of regeneration your drive will frequently trip with DC link overvoltage fault. I am sure this will not be acceptable to you. So you need to go for a MM440. or second option is you connect abraking unit but this will be not be economical. diwa. |
Follow us on