1/5/2017 7:26 PM | |
Posts: 30 Rating: (5) |
Hi David, here's a list of recipes for Yocto Krogoth that can be added when building: http://recipes.yoctoproject.org/rrs/recipes/2.1/All/ , perhaps the usbutils recipe is what you're looking for. I think you can also do opkg list to see if it's available that way, but it looks like you already looked indirectly. If you want to build a new image with that recipe, you'd add it to this file: https://github.com/siemens/meta-iot2000/blob/master/meta-iot2000-example/recipes-core/images/iot2000-example-image.inc during the build procedure. HTH, Jake |
1/9/2017 4:13 PM | |
Posts: 40 Rating: (2) |
Hi, The "cdc thing" is installed here: https://github.com/siemens/meta-iot2000/tree/master/meta-iot2000-example/recipes-kernel/acm-gadget What exactly is your problem? Do you have any errors? The serial port for the cdc acm is ttyGS0 which is directed to the micro usb port. Is this what you are looking for? |
This contribution was helpful to1 thankful Users |
Follow us on