3/7/2017 11:48 PM | |
Posts: 4 Rating:
|
------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 3/8/2017 4:35:30 PMNew subject after splitting |
|
3/9/2017 11:17 AM | |
Joined: 10/18/2012 Last visit: 8/21/2024 Posts: 225 Rating:
|
Maybe I'm completely wrong, but doesn't the IOT2040 require 24V instead of 12V? |
3/23/2017 11:03 AM | |
Posts: 4 Rating:
|
I returned it to my supplier. |
3/23/2017 12:33 PM | |
Posts: 531 Rating:
|
Was the sd card correctly inserted and which usb port did you use? Did anything show up in hardware manager on windows side? |
I was wondering someone could help me, because the online community support is quite limited at this moment. I'm the lucky owner of a IOT2040 :) However, I got a problem with getting it recognized on a Windows PC.
My device manager can't find the device.
I'm trying to program the intel Galileo gen 2 with Arduino IDE.
I already installed the intel packages for the intel galileo.
It's powered by 12V/1A and the only other the connection is the USB micro ---> USB Windows PC.
Please help :)