4/10/2017 1:14 PM | |
Posts: 9 Rating: (1) |
I need to include some libraries to my Eclipse proyect. In this case the library I want to use is called LiquidCrystal, which allows to easily manage LCD screens compatible with Arduino. (Source code available here: https://github.com/arduino-libraries/LiquidCrystal) I cant include/link this library (other neither) with my proyect. I tried copy-pasting the cpp and hpp files into my proyect, but it seems those files need access to other libraries as well (See attachment) How can I use external libraries in my proyects? |
Last edited by: bamsbamx at: 4/10/2017 1:15:47 PM |
|
4/10/2017 1:45 PM | |
Posts: 71 Rating: (16) |
This library is designed to be used in the Arduino environment and therefore depends on other Arduino libraries (Print.h). You can either use the Arduino capability of your IOT2000 or try to port the Print library yourself. The problem itself has nothing to do with using external libraries in your Eclipse project. |
4/10/2017 2:09 PM | |
Posts: 9 Rating: (1) |
Thanks for the answer, but did not understand properly. By saying 'use the Arduino capability of your IOT2000' you mean using the Arduino IDE to develop for the IOT2000? |
Follow us on