4/14/2017 4:24 PM | |
Posts: 2 Rating: (0) |
anyone listening.... Here's my sketch (using Arduino IDE). basic 0.96" OLED display +5 to IOT2040 5V display will not show anything. Anyone have and idea to to get this working? I can get a blink and PWM to illuminated and LED, but not a simple display. #include<Wire.h> #include<SeeedOLED.h> #include<avr/pgmspace.h> void setup() { Wire.begin(); SeeedOled.init(); //initialze SEEED OLED display SeeedOled.clearDisplay(); //clear the screen and set start position to top left corner SeeedOled.setNormalDisplay(); //Set display to normal mode (i.e non-inverse mode) SeeedOled.setPageMode(); //Set addressing mode to Page Mode
SeeedOled.setTextXY(0,0); //Set the cursor to Xth Page, Yth Column SeeedOled.putString("Hello World!"); //Print the String } void loop() { } |
4/18/2017 7:24 AM | |
Posts: 71 Rating: (16) |
Are you sure this does even compile? You are including libraries for AVR microcontrollers (avr/pgmspace.h) there. |
Follow us on