2/21/2017 12:45 PM | |
Posts: 8 Rating:
|
Dear all. I'm trying to use Kepware server. I can see the change of variables in PLC (Not Simulation) But, when I use PLCSIM, OPC's variables don't change.. Kepware's Communication quality is good, but when i change variable, it doesn't changed in Kepware. I tried many things such as looking for YOU_TUBE, but i can't solve... Can you let me know how to solve this problem? and, I have questions. 1. Do I have to Set Something in kepware before using PLCSIM? (with another tool) 2. Do I have to build & download H/W configuration? 3. My TCP/IP is not connected. I use Default Network. I think it is not necessary. is it right? Thank you.
AttachmentPictures.zip (293 Downloads) |
This contribution was helpful to
1 thankful Users |
2/21/2017 4:30 PM | |
Posts: 8 Rating:
|
Thank you. I download NetToPLCsim. But... PLCSim is connected, but Client (PORT 102) is not connected. I set my computer's IP as 192.168.0.1, but there are just Wireless Internet IP... I think, because my TCP/IP is not connected somewhere. Should I type something in 'cmd'? Here are my S7 and NetTPLCsim version. Please. AttachmentPictures (2).zip (398 Downloads) |
Last edited by: strmin123 at: 2/21/2017 4:30:52 PM |
|
4/20/2017 6:11 PM | |
Posts: 1 Rating:
|
Port 102 shall be fixed. Try change firewall setting. |
Follow us on