10/9/2017 4:59 PM | |
Joined: 9/27/2006 Last visit: 7/31/2024 Posts: 12272 Rating:
|
Hello Steve; The only integrated safety function available in the G120C is STO (safe torque off). See the table below, taken from the following manual: Safety Integrated - SINAMICS G110M, G120, G120C, G120D and ... The manua;l has chapters describing the STO function (section 3.7.1), showing how to wire the G120C for STO to SIL 3 (see 4.4.3) or command it over Profibus/Profinet , and how to evaluate it cyclically to maintain the SIL 3 certification, see section 6.2.1. Hope this helps, Daniel Chartier |
Follow us on