7/20/2016 8:50 PM | |
Posts: 106 Rating: (2) |
Hi I'm using a Step 7 v5.5 and I did the configuration of the OPC server for S7 connection on the page 104 (https://support.industry.siemens.com/cs/ww/en/view/13542666), so I can use a symbols. I tried to add a DB access(R/W) with configured and all symbols, but in the opc scout I can only see the symbols that are in the symbol table. The DB I tried to add has it's own symbol name and it is listed in the symbol table, but it can't see it in the OPC scout (SYM/SIMATIC(300)/CPU 315-2 PNDP) How can I add DB so they can be visible in the OPC scout by a symbolic name? ------------------------------------------------------------------------------------------ |
Last edited by: dolbyinside at: 7/20/2016 8:58:32 PMLast edited by: Min_Moderator at: 7/21/2016 2:20:16 PMReplace link Last edited by: Min_Moderator at: 7/21/2016 2:21:45 PMNew subject after splitting |
|
11/15/2017 2:53 PM | |
Joined: 6/19/2017 Last visit: 8/5/2024 Posts: 8175 Rating: (169) |
New question published by ms23 is split to a separate thread with the subject Need to add another DB to OPC Scout server by a symbolic name . Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on