Industry Online Support
Technical Forum
7/9/2008 9:16 AM | |
Joined: 4/24/2006 Last visit: 10/2/2024 Posts: 8743 Rating: (1168) |
Hi, Do you scale the analogue input? Best regards, Wizard |
7/9/2008 3:12 PM | |
Posts: 5 Rating: (0) |
I have made the scale as the factory seting 0-10 volts means 0-50Hz there is nothing related to the scaling |
7/9/2008 3:55 PM | |
Joined: 4/24/2006 Last visit: 10/2/2024 Posts: 8743 Rating: (1168) |
Hi, I guess you have put dipswitch in right position? What value has P2000? Best regards, Wizard |
7/11/2008 6:46 AM | |
Joined: 5/21/2008 Last visit: 8/27/2024 Posts: 91 Rating: (0) |
i think you have not linked terminal 2 & 4. It is a must when using apotentiometer. pl. check. |
Follow us on