1/27/2018 9:16 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating:
|
Hello, From your description, it seems that Drive is controlled via PLC+HMI. You need to study PLC logic as well as HMI configuration, i.e. how motor speed is set via HMI, communication between HMI ---> PLC ----> to drive etc. etc. BTW, is it new machine under commissioning or old running machine. Please study below application example to understand the project well. SINAMICS G: Speed control of a G110M/G120/G120C/G120D using S7-300/400F (STEP 7 V5) with PROFINET/PROFIBUS and Safety Integrated and HMIHTH. |
Last edited by: Jen_Moderator at: 1/29/2018 9:49:42 AMInserted right link. |
|
1/29/2018 8:18 AM | |
Joined: 3/31/2015 Last visit: 1/26/2024 Posts: 175 Rating:
|
285.000 should work. |
1/30/2018 8:39 AM | |
Joined: 6/19/2017 Last visit: 6/28/2024 Posts: 8176 Rating:
|
New question published by ndosh is split to a separate thread with the subject Have difficulty to change value P1080 during run condition. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on