3/11/2018 2:02 PM | |
Joined: 7/23/2016 Last visit: 4/29/2024 Posts: 37 Rating: (0) |
dear all could any one help me i have a problem in one D425 CPU , it doesn't working normally and the notification LEDs as showing in the photo RDY is green DPT is green but the others are off , and the seven segment is showing number 6 in my machine there is different status as the following RDY , RUN , DP1 , DP2 all are green and the others are off , and the seven segment is showing number 6 ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/12/2018 3:15:59 PMNew subject after splitting Ahmed Atef |
|
3/15/2018 8:18 AM | |
Joined: 10/11/2006 Last visit: 9/30/2024 Posts: 5909 Rating: (806)
|
Hello, please see chapter 9.1. When the dot beside the 6 is blinking, the Simotion is powered on and you can do further diagnose via Scout or see Chapter 9.3.2. https://support.industry.siemens.com/cs/ww/en/view/109749954 |
With best regards, |
|
Follow us on