(0)| 6/21/2018 11:16 AM | |
|
Posts: 28 Rating:
|
hii can you share the programming for timer on S7-300 CPu 315 on simatic manager and WIncc 7.2 I am unable to get the Timer from mili second to seconds even after doinglinear scalling on wincc Tag. Used as 16 Bit and 32 Bit both ways ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 6/22/2018 8:50:54 AMNew subject after splitting |
|
| 6/22/2018 11:06 PM | |
|
Joined: 11/5/2012 Last visit: 8/14/2025 Posts: 490 Rating:
|
Hello Richie_Goel, good day. Do you want to convert from S5time format to seconds? If that's the case, I'f suggest you to first convert from S5Time to time and then do a scale to seconds, dividing the Time value by 1000, since Time format is given in miliseconds. To convert from s5Time to Time, I see you are using a S7300, you have avaiable the standard library, IEC function blocks subfolder, the FC33 "S5TI_TIM" this one converts from S5Time to Time format. then do the calculation of Ms to seconds. I hope this is what you need and helps your. Regards. |
Follow us on