7/27/2018 4:22 PM | |
Joined: 12/18/2014 Last visit: 7/27/2024 Posts: 33425 Rating: (4148)
|
You can not upload anything to the TDE, only to a basis module. |
7/27/2018 4:56 PM | |
Posts: 15 Rating: (0) |
Yes I tried that aswell. Sorry but I still cannot manage to communicate. Thanks for your help |
7/31/2018 7:05 AM | |
Joined: 2/20/2014 Last visit: 7/19/2024 Posts: 396 Rating: (38) |
Hi pompagarage, If you are expecting a proper solution, it is better for you to upload the file (if you are not ready to upload actual program file, then please proceed to create another separate program file (just with one or two lines of circuit program) & configure the message text to be displayed on both base module & TDE (can you also provide the photo of the IP setting done on the base module & TDE (to capture & upload a photo will not take a very long time). Please appreciate that ixo65 is taking all his time replying to your every post & after so many posts you are not taking the effort to provide any program file.screenshots/photos. This is not the right way to repeatedly post your query without providing the full information requested by the person who is volunteering to support you. |
Follow us on