(0)| 8/17/2018 2:37 PM | |
|
Posts: 1 Rating:
|
hi am new in drive programming i have confugen how to programed g120 drive with status and control word using starter software and plc s7 ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 8/20/2018 8:51:58 AMNew subject after splitting |
|
| 9/25/2018 8:00 PM | |
|
Joined: 10/13/2017 Last visit: 4/8/2025 Posts: 4 Rating:
|
Assuming you have access to TIA Portal. The G120 can be programming using startdrive within. I would suggest using the given blocks and Technology Objects to make things way simpler in code. Also there is a block called SINA_Speed which can be used if you do not wish to use Technology Objects. In TIA Portal when you configure your telegram, there are tags (STW, ZSW) that are created in the default tag table which will allow you to directly control the drive over telegram. You will have to determine which bits are required for your application, and write the Hex value directly to the words. You can alternatively configure the bits in the control and status words as Bool tags and control them independently of each other. See the list manual for your specific drive and locate the section for the Internal control/status words (e.g. pg. 548). I particularly think the Sequence Control - Sequencer chart on pg. 564 may also be of use for you. Applcation Example which demonstrates using SINA_SPEED Function Block. If you do not have access to TIA Portal, and are using S7 Classic, the guide below will help. Guide for S7 with field busses and Starter (See Chapter 3 pg.15) |
Last edited by: dlevine at: 9/25/2018 8:02:18 PMLast edited by: dlevine at: 9/25/2018 8:02:50 PMLast edited by: dlevine at: 9/25/2018 8:06:07 PMoptimized links |
|
This contribution was helpful to
|
|
Follow us on