10/1/2018 7:09 PM | |
Joined: 2/22/2017 Last visit: 7/11/2024 Posts: 24 Rating:
|
Hi everyone, i had one hardware connecting as below" Thermalcouple --> transmiter 4-20mA ---> Analog input Wago 750-474 (connect to pin with hardware address is PIW176 ) --> PLCs7 300 via profibus. all values of Thermal to save data base DB24.DBD16 , i found all progams PLC but i didn't find out any Function Block to get PIW176 to DB24.DBD16, because i want to modify a bit in Formula, on the line 31812 (STL source - attachment file) only one, Could you please help me to find out which Function block containt moving data from Wago module to DB24.DBD16, please see my attachment file, Thanks & regards, huynhhai77 AttachmentSTL.TXT (59 Downloads) |
10/2/2018 11:12 AM | |
Joined: 2/22/2017 Last visit: 7/11/2024 Posts: 24 Rating:
|
Dear RIAN Che, I attachment PLC program, please refer to it Regrads, huynhhai77 AttachmentMyprogram.zip (56 Downloads) |
10/15/2018 9:57 AM | |
Joined: 2/22/2017 Last visit: 7/11/2024 Posts: 24 Rating:
|
Dear Willybong, Thanks for your help, I unlocked protect function block FC161 and FC166 also but I didn't find out any position data transfer to DB24.DBD16, I want to modify a little data before transfer to DB24.DBD16, Could you test force valve with input analog PIW176 ( when you increase value over 127 decimal, it will return negative value, I don't know why), DB24.DBD16 to display actual value on Intouch Wonderware SCADA, Could you please check programs again with unlock function block, see my attachment file Thanks and best regards, huynhhai77 Attachmentunlock_protected_myplc.zip (57 Downloads) |
Follow us on