11/6/2018 7:56 AM | |
Joined: 4/28/2015 Last visit: 11/5/2024 Posts: 3345 Rating: (379)
|
Hi, for Modbus and TCP/IP protocol you can use for example node-red to read/write data from/to the climatix controller. There is also a node for bacnet communication We do not have any example for this kind of protocols. But if you search for node-red in the forum you will find some entries with information regarding that. Using the tcp node is not that difficult, just have a look at the tcp-node in node-red. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
11/11/2018 6:25 PM | |
Joined: 4/28/2015 Last visit: 12/19/2023 Posts: 2 Rating: (0) |
Hello, Please specify: Climatix controller type, firmware version, extension modules... Cllimatix range has many communication options:KNX, KNX/IP, Bacnet/MSTP, Bacnet/IP, Modbus serial, Modbus TCP, JSON, rainbow, etc.... BTW: do you know climatix has a cloud solution too ? (www.climatixic.com) You can use cloud or cloud API or device API.... I don't really understand Desigo part of your question BR, Zoltan |
This contribution was helpful to2 thankful Users |
Follow us on