9/12/2018 3:32 AM | |
Posts: 4 Rating:
|
Hello HugoD, Thank you so much for the answer! I think there's a link from which you can download the latest version MindConnect LIB. It includes an application example, but hasn't a detailed instruction. Yes, MIndConnect Nano or IOT2040 will be the perfect method to connect MindSphere cloud platform, but for now it only supports OPC UA & S7 for connecting field devices . In my case, I need to connect devices with other communication protocols, for example Modbus/TCP. So, the SIMATIC IOT2040 with MindConnect LIB is a suitable solution for me. |
11/12/2018 7:57 AM | |
Joined: 4/28/2015 Last visit: 8/26/2024 Posts: 3345 Rating:
|
Hi, have a look here Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on