1/14/2019 11:49 AM | |
Posts: 3 Rating: (0) |
Parameter P648 = 9. In the attachment recording of signals. I compared the parameters of both drives. They differed only in the Profibus address, but one does not work. I confused by the lack of alarm messages.
AttachmentdriveB .pdf (181 Downloads) |
Last edited by: Victor_R at: 1/14/2019 12:01:12 PM |
|
1/14/2019 12:10 PM | |
Posts: 3 Rating: (0) |
Attached is a screenshot with parameters. |
1/14/2019 12:27 PM | |
Joined: 8/25/2006 Last visit: 8/25/2024 Posts: 2208 Rating: (278)
|
The source of OFF2 command could be also E-STOP from terminals 105 or 107. Look at function diagram G117 and G180. |
Follow us on