10/6/2016 9:39 AM | |
Posts: 1 Rating:
|
Dear Gents, Sorry to raise up this topic, since there is no solution from previous topic about PROFIBUS Connection simulation in PLCSIM. I try to simulate Profibus DP between two CPUs in PLCSim but it didnt work, there was no data transfer happened. #I am attaching the project overview (via gdrive) 1. Network Overview 2. Master STN Hardware Config 3. Slave STN Hardware Config #Program Config : 1. Master STN - OB1, OB82, OB86 OB1 Program For Master Station
2. SLAVE STN - OB1, OB82, OB86 OB1 Program For Slave Station
I am attaching PLCProgram also, as well PLCSim files. is there missing configuration made by me? need your advice? Program used : 1. Step 7 V 5.5 AttachmentFiles.zip (391 Downloads) |
Last edited by: helmiwg at: 10/6/2016 9:42:11 AMLast edited by: helmiwg at: 10/6/2016 9:44:13 AMLast edited by: Min_Moderator at: 10/6/2016 10:35:36 AMAdd attachment |
|
10/6/2016 7:21 PM | |
Joined: 3/14/2016 Last visit: 9/1/2024 Posts: 162 Rating:
|
It is possible to communicate with PLCSIM using ISO TCP over port 102, it has to be done with a third-party software, although. The NetToPLCSim Project make it possible. I use it on a VM with bridged adapter and I'm able to communicate my SCADA with the PLCSIM for testing. |
"Engineers like to solve problems. If there are no problems handily available, they will create their own problems." (Scott Adams) |
|
This contribution was helpful to
2 thankful Users |
Follow us on