6/4/2019 12:21 PM | |
Joined: 5/13/2016 Last visit: 1/15/2022 Posts: 66 Rating: (5) |
Hi, Electrical diagrams are (of course) completely depending on what you want to achieve with your set-up. I did however include some basic drawings I've made for a simple system with some dimmable lights (with the use of NIKO dimmers) and "normal" lights (on/off) controlled via switches. Also you will find some Alarm Sensor inputs (marked as AS) and a day / night sensor (marked as E1). Also there is a buzzer (Z1) and an alarm horn (Z2). I left out all the comments as these are in the Dutch language, not sure they will help :) Again, it's just a simple drawing but perhaps it will help. AttachmentPanel 1.zip (278 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on