4/11/2006 9:43 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (318) |
Hi, The way to communicatie is withProfibus FDL by using the SEND FC5 en RECEIVE FC6, the connection have to be aranged in Netpro between the two CP443-5. In the next link is a example for a Ethernet link, but this software is also working for Profibus FDL: http://support.automation.siemens.com/WW/view/en/17853532 |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
4/12/2006 8:18 AM | |
Posts: 9 Rating: (1) |
Is FDL not an old way of S5 communication? isn't the lowestlayer of communicating. Is it fast enough? best regards |
Follow us on