7/8/2019 6:11 PM | |
Joined: 11/8/2017 Last visit: 10/16/2024 Posts: 338 Rating: (192) |
Hi, Apart from the usual networking / IT security considerations, integrating this device directly into either Desigo CC or Desigo Insight should not be an issue. CC has a good method for auto-discovery of 3rd party devices and points. The process to integrate to CC is fairly straight forward. Desigo Insight is similar, but different. The PICS statement is attached for the Wago device. The only issues you may run into would relate to the 3rd party device BACnet conformance - i.e. something doesn't work quite as it should (i.e. a Schedule can be Read into CC - but can not be Written to from CC). Some devices will be perfect, some will have issues though. Regards, AttachmentPICS_t07500831_xxxxxxxx_0en.pdf (342 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on