(0)| 6/8/2007 8:50 AM | |
|
Posts: 75 Rating:
|
Whether probably to diagnose a condition the power supply PS407 10A CPU414-4H in user program? |
| 6/9/2007 4:16 PM | |
|
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
Hi Dimbas, See the source in STL to compile directly. You can read out with OB81 that there are power-failures and detect for example that the batteries are empty. This block will work for 4A power supplys also. AttachmentCheckPS.zip (585 Downloads) |
|
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
| 6/24/2007 12:58 PM | |
|
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
Hi Aret, You may make the amount of diagnostic messages bigger in the hardware, by placing also OB85 to "only for incoming and outgoing messages" and throw OB121/122 out of the program you may see which message is transfered to the diagnostic buffer. There is also a SFC where you can read out the diagnostic buffer from the program. See System Software for S7-300/400 System and Standard Functions to read out the diagnostic buffer. In the chapter 33.30 SSL-ID W#16#xyA0 - Diagnostic Buffer you can read-out more information how to do that. In STEP7is the structure of the diagnostic data explained. Keep me posted... |
Last edited by: Late at: 24.06.2007 13:04errors in text I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on