3/31/2020 7:30 PM | |
Posts: 46 Rating: (0) |
Hi, I have the folowing application: control a valve (4-20mA) so that the delta T between the in and out temperature of a heatpump is around 2°C. T in and out is mesured by 2 sensors 0-100°c 4-20mA The system shoud not react fast to prevent wear on the valve actuator Hope someone can help me on the way. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/01/2020 09:47:28New subject after splitting |
|
3/31/2020 7:39 PM | |
Joined: 12/18/2014 Last visit: 7/26/2024 Posts: 33420 Rating: (4148)
|
Hello Yves-M, what is it for a valve? A proportional valve? A mixing valve? |
Follow us on