6/23/2020 8:57 PM | |
Posts: 1 Rating: (0) |
hello sir hope youre good there , we have a uprightTL38 machine but we are having a problem with the machine DC Motor , the problem is that the power of the motor is lower he canot rotate free way when we take controls up and down we see that the power of motor started to go low we canot use it and after 10 minutes the motor start to work propertly please help mee im having a serious problem ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/24/2020 09:36:50New subject after splitting |
|
6/24/2020 8:11 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (875)
|
Hello, You have post your query in wrong post. If it is DC motor with Siemens DC drive, you should post in DC converters SIMOREG product conference. BTW, how this DC motor is controlled? which is drive? Do you see any alarm or fault code on drive? Please provide motor nameplate, drive details, application etc. etc. |
Follow us on