10/7/2020 7:44 PM | |
Joined: 12/18/2014 Last visit: 7/24/2024 Posts: 33412 Rating:
|
Do you have any idea what the LOGO! can and how you could realize your challenge? |
10/14/2020 11:00 PM | |
Joined: 2/22/2008 Last visit: 6/12/2024 Posts: 2698 Rating:
|
Your desired function is possible depend on the starts per hour, see attachment for example. For each start you increase the counter and starts an additional timer with 60min. If the time is over, you decrease the counter. In the example the timer setup is 60s for simulation, change it later to 60min. You have 8 timers for a maximum of 8 starts per hour. If it is not enough, then expand the program by copying the lines with the timer and other blocks, prefer a 4 lines block. You can see, the memory will grow up, if you have 16/32/64 starts per hour. Therefore the questions from other members, what you really want. Maybe there are other solutions in a similar way with less blocks, this was my first idea. Regards, Scorp AttachmentLast60min.zip (104 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on