10/30/2020 8:37 AM | |
Joined: 1/4/2007 Last visit: 10/11/2024 Posts: 1146 Rating: (175)
|
Hello mraheem, If the LED „LC“ is not green: That means, your load cell isn’t connected correctly to the WP231 module. Into the manual of the WP231, you can find in chapter 6.4.2 how to connect a load cell to the WP231 module: https://support.industry.siemens.com/cs/ww/en/view/109780855 Best regards Siwarexi |
This contribution was helpful to1 thankful Users |
10/30/2020 2:15 PM | |
Posts: 12 Rating: (0) |
I attached photo for SWAREX when i Connected it with Load cell |
10/30/2020 2:17 PM | |
Posts: 12 Rating: (0) |
I attached photo for SWAREX wire diagram with Load cell If LC is red that is mean the load cell is damaged ? |
11/3/2020 2:02 PM | |
Posts: 12 Rating: (0) |
Thank you , My Load Cell is Damaged |
Follow us on