11/25/2020 1:27 PM | |
Posts: 1 Rating: (0) |
Hallo Mr, I already connected 3 meter MAG5000 using digital input (terminal 56 & 57) with datalogger. The problem is the flowrate in the logger is not same as reading in meter? For example in meter 200 l/s in logger 160 l/s. Any suggestion? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/26/2020 09:17:05New subject after splitting Last edited by: Jen_Moderator at: 11/26/2020 09:17:41Optimized headline. |
|
Follow us on