7/22/2019 10:28 PM | |
Joined: 1/3/2019 Last visit: 12/16/2022 Posts: 64 Rating: (0) |
Hi frends.. I have a logo8 and one hmi ktp700, i decide to connect another hmi to other place.. about 100m is distance beetwen two hmi... how i can do it with lan cable? Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/23/2019 06:59:31New subject after splitting En. M.ABZADEH |
|
7/23/2019 4:39 AM | |
Joined: 12/18/2014 Last visit: 8/8/2024 Posts: 33513 Rating: (4163) |
Hello M.Abzadeh, the manual says the max. length is 100 m with CAT5e cable. See attachment. AttachmentLOGO! 8 manual 0BA8 2017_11 xxxx8-0BA0 page 319.pdf (177 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on