1/1/2022 4:31 PM | |
Joined: 1/12/2018 Last visit: 11/4/2024 Posts: 3 Rating: (0) |
I have (with some success) used SIEMENS TCP File Server (v 2.0) to write log files from PLC S7-1214C to Windows PC instead of PLC MC. The log files are of two types: However, errors occur when initializing the communication: 1. At first connection after program load, the deafult File name is used instead of the supplied name. Presumably because no client table has been created yet. 2. Connection is governed by the "enable" bit. Attached: AttachmentPrepare TCP.txt (499 Downloads) |
Follow us on