3/28/2021 1:35 PM | |
Joined: 2/6/2021 Last visit: 1/1/2022 Posts: 7 Rating: (0) |
|
3/28/2021 1:39 PM | |
Joined: 2/6/2021 Last visit: 1/1/2022 Posts: 7 Rating: (0) |
I should see an error output when the connection drops |
3/28/2021 1:43 PM | |
Joined: 2/6/2021 Last visit: 1/1/2022 Posts: 7 Rating: (0) |
All I want is to get an error when the connection drops |
3/28/2021 5:15 PM | |
Joined: 9/21/2012 Last visit: 5/19/2024 Posts: 3944 Rating: (445) |
You should use the forum search, it's a very powerfull tool. Hint: use DeviceStates as the search criteria. |
3/29/2021 10:36 AM | |
Joined: 6/19/2019 Last visit: 5/10/2024 Posts: 694 Rating: (73) |
Maybe there are option to do watchdog and then you will see then Profinet will be broke? |
Follow us on