7/10/2023 6:20 AM | |
Joined: 7/8/2023 Last visit: 8/22/2023 Posts: 8 Rating: (0) |
Hello Our 840d device (according to the attached picture) first gave a battery message and then a message of no connection of NC / PLC. Also, the condition of the lights is according to the attached figure Please help me Thank you
AttachmentScreenshots.zip (296 Downloads) |
Last edited by: ALNR at: 07/10/2023 06:58:14Last edited by: ALNR at: 07/10/2023 07:04:04Last edited by: Jen_Moderator at: 07/10/2023 12:52:25All files added as .zip file. |
|
7/10/2023 12:21 PM | |
Joined: 5/24/2016 Last visit: 8/8/2024 Posts: 346 Rating: (52)
|
Battery died and the machine has lost it's memory. Do you have a backup of the machine? |
7/11/2023 5:22 AM | |
Joined: 7/8/2023 Last visit: 8/22/2023 Posts: 8 Rating: (0) |
thanks a lot Shouldn't I replace the battery first? And is there a backup version on the hard drive?
|
7/11/2023 7:50 AM | |
Joined: 7/8/2023 Last visit: 8/22/2023 Posts: 8 Rating: (0) |
Sorry What does this mean? the POK is on the PR is off and the PS is blinking. also the PF is on as the picture |
Follow us on