1/17/2020 12:22 PM | |
Posts: 95 Rating: (0) |
done as you said. nc cleared and downloaded after that plc data cleared and downloaded but same issue. |
1/17/2020 12:55 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (874)
|
Could you please attach your NC.ARC file here? It will help to understand your machine configuration. |
1/18/2020 5:01 AM | |
Posts: 95 Rating: (0) |
sir back up is saved in 840d hard disk.how to take it pen drive.any setting need for this sir. |
1/18/2020 5:42 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (874)
|
Is your USB port on PCU20/50 is activate? Check if pen drive is detected when it is insetrted in port. If yes, while taking series start up back up, select the path of pen drive to save back up. If above doesnot work, I suggest you to take DATA back up on external PG/PC. For that you need external PG/PC with RS232 port or USB to RS232 adopter plus WINPCIN software. With this you can take backup. Please refer attached file & take START UP data back up & attach here. AttachmentData_Loading_through_WINPCIN.pdf[1].pdf (154 Downloads) |
2/7/2020 8:34 PM | |
Posts: 110 Rating: (3) |
Hi dear Do not worry plz take pics of screen and post here after inter in service, then Press Data IN , Here you can see two thinks ( soft keys) 1. NC cad 2 Archive 1st of all press NC card if any file show then take picture and post if nothing than back in services and press key Archive take picture then we tell you next procedure Shortly here you can select file and restore to system according previous post in attached PISCEAN 2010 and Sir NULIZHANG Posts Hope full you can do this and finally solve the issue With best wishes Rana Ali Attachment840d PL NC___PLC_Data_Clear & restore procedure.pdf (148 Downloads) |
Last edited by: Rana Ali at: 02/07/2020 20:41:17Last edited by: Rana Ali at: 02/07/2020 20:43:30Last edited by: Rana Ali at: 02/08/2020 06:08:11 |
|
Follow us on