7/25/2024 9:11 AM | |
Joined: 11/21/2020 Last visit: 11/7/2024 Posts: 179 Rating: (0) |
Hi, In attachment you'll find short program for RPM measurement which I saw on Youtube. The guy is using 1200 PLC and Beckhoff 05.2420.1230.1024.5009 HTL encoder, I have tried to repeat the same using Baumer's and Pepperl's HTL encoders (Pepperl's 10-11651_R-1200datasheet is in the pdf attached), but in my case counter doesn't reset to 0 after shaft stop. Can someone say what is the problem, is this genius just a fraud (maybe he just cuts encoder's power supply or something else)? Is the formula in his video correct Speed (rpm)=[Value of Encoder (frequency) / Encoder Resolution] *60 Can someone share similar program for HTL encoder, where counter automatically resets after shaft stop? AttachmentBinder1.pdf (290 Downloads) |
Follow us on