3/20/2017 8:54 AM | |
Joined: 5/28/2008 Last visit: 12/1/2023 Posts: 1343 Rating:
|
Can you please send us the MLFB of the PLC and the TIA Version you are using? |
3/20/2017 1:55 PM | |
Joined: 1/30/2006 Last visit: 11/28/2023 Posts: 310 Rating:
|
Hi Here is text from the manual: Uploading the safety program to a programming device or PC (S7-1200, S7-1500) The "Load from device" function is not possible for S7-1200/1500 F-CPUs for safety programs. You can download individual F-blocks to a PG-PC. This also applies to standard CPUs with F-I/O in standard mode. Manual, see page 286 BR.- Sven |
BR. Sven |
|
3/21/2017 7:33 PM | |
Posts: 3 Rating:
|
Ok thx that can make sens. Than how i can upload F-blocks individual? I need to remove safety signature and than i can upload it? |
Follow us on