3/12/2007 4:30 PM | |
Posts: 2 Rating: (0) |
Ok, I found it myself, its in the hardware catalogue under 'Additional field devices' > 'I/O' > 'ET200M' |
8/12/2007 3:53 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (318)
|
Hi Henio, Which Version of STEP7 did you have ? You need at least version V5.4... this because you can use this 2BA01 also for redundant communication with a H-System and also for the PA-link and the Y-link. This year there will be also a -2BA02 where you might use 12 modules behind the IM153-2BA02. AttachmentIn the Profibus DP under ET 200M is in STEP7 Hardware configuration the IM153.pdf (229 Downloads) |
Last edited by: Late at: 12.08.2007 15:54HSP 0085 is the Hardware Support Package for this IM153-2BA01.... I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on