9/4/2016 4:20 PM | |
Joined: 11/7/2014 Last visit: 7/24/2024 Posts: 12 Rating: (1) |
Dear PISCEAN 2010, You can copy paste the link to mediafire to download? 1/ In my opinion the NCK backup is good because after i reload it the machine config is right (5 axis, drive modules recognized) 2/ The steps are as in this guide: https://support.industry.siemens.com/tf/ww/en/posts/reset-cpu-plc-for-840c/59093/?page=0&pageSize=10 3/Yes its the same error before and after resetting+reloading data. Below is the PLC program only. AttachmentS5_DATEN.zip (82 Downloads) |
Last edited by: quangnguyen.digicnc at: 9/4/2016 4:21:15 PM |
|
7/31/2024 12:46 PM | |
Joined: 7/30/2024 Last visit: 8/2/2024 Posts: 54 Rating: (0) |
New question published by AutoGen_2536864 is split to a separate thread with the subject 840C Index G300 Lathe: PLC file size "0". Best regards |
Follow us on