5/19/2017 8:56 AM | |
Joined: 4/13/2013 Last visit: 11/26/2021 Posts: 12 Rating: (0) |
Dear All, I am in a kind of mess. I want to replace OP7 with KP700 Comfort using TIA portal v13 but this migration is not directly possible. I have to first convert OP7 program to WinCC Flexible 2008 and only that program can be migrated into TIA Portal. I don't have time on my side to buy WinCC Fleixble 2008. Even if I get it, I don't know how much problems it will create while installation on a computer that already has PCS7 v8.1 and TIA Portal v13. Can anybody here migrate this .pdb file to WiCC Flexible 2008 that I can migrate in TIA Portal v13? I will be really grateful for this favor. I hope I am not asking for too much. OP7 file is attached. AttachmentKK22CB.zip (421 Downloads) |
5/19/2017 10:29 AM | |
Posts: 8946 Rating: (999) |
I checked the file... L2-DP Communication IS NOT Supported any more, OP7 also of course. You have to change your Hardware and your Panel if you like to use TIA! I change to S7-300 and 177B for the migration... AttachmentK22CB_V13_SP1.ZIP (487 Downloads) |
This contribution was helpful to1 thankful Users |
5/19/2017 10:45 AM | |
Posts: 8946 Rating: (999) |
Dear, please read my answere here from 5/19/2017 10:29 AM. |
5/20/2017 6:33 AM | |
Joined: 4/13/2013 Last visit: 11/26/2021 Posts: 12 Rating: (0) |
Its version v13 SP1 Update 9. Check attached file please. |
Follow us on