10/4/2017 6:08 AM | |
Joined: 11/18/2010 Last visit: 8/11/2024 Posts: 14 Rating: (0) |
Dear all, Could anyone know about permitted transfer distance for current signal 4-20mA of Transmitter? I am using pressure transmitter SITRANS P220, the distance from transmitter to PLC module is about 450m, is it possible to connect current signal of transmitter directly to PLC module? In case of using repeater, which one should be chosen and how many repeater needed? Please refer attachment for P220 specification. AttachmentP220.pdf (1119 Downloads) |
6/27/2024 4:19 PM | |
Joined: 10/9/2023 Last visit: 6/28/2024 Posts: 1 Rating: (0) |
Hi, Good explanation! How did you calculate the distance for 450ohms? |
6/28/2024 8:22 PM | |
Joined: 3/28/2010 Last visit: 8/5/2024 Posts: 1051 Rating: (212)
|
450 Ohms is the resistance of what? |
Follow us on