2/22/2018 1:12 PM | |
Joined: 8/3/2009 Last visit: 8/15/2024 Posts: 13561 Rating: (1713)
|
Hello jmlai Here a FAQ with the Answer: https://support.industry.siemens.com/cs/de/en/view/61883659 there is a note: "Note Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
8/19/2022 4:17 PM | |
Joined: 2/17/2022 Last visit: 5/15/2024 Posts: 3 Rating: (0) |
Hello jmlai Although some users say:
it is possible to read / write data from MS SQL Server via VBScript on Siemens HMI. I tested below code on simulation for TP1200 Comfort PRO and it works !!!
I hope it helps... Also look: https://automationscript.com/uft/vbscript-to-connect-to-sql-server-and-run-query/ Barış |
This contribution was helpful to1 thankful Users |
8/30/2022 8:45 AM | |
Joined: 8/3/2009 Last visit: 8/15/2024 Posts: 13561 Rating: (1713)
|
Hello Baris Yes you have testet it in SIMULATION that is running on a PC. Here the Script objects of the PC are available. But this will not run on a Real Panel!! In this case you have to consider the local ressources and script functionalities of the Panel. Bye Murof |
Last edited by: Murof at: 08/30/2022 08:45:32Last edited by: Murof at: 08/30/2022 08:45:57If this Information really helps, you could use the Rate function |
|
9/2/2022 7:56 PM | |
Joined: 2/17/2022 Last visit: 5/15/2024 Posts: 3 Rating: (0) |
Hi Murof, Ok, some of my friends also told me, in spite of it runs on simulation, it doesn't work on real HMI hardware. In the first place, that script i wrote above which is running on simulation, communicates the SQL server on the same local computer as with the simulation. That could introduce some troubles when using real Siemens HMI. So, i don't want to mislead the users, this works on simulation, not on real HMI panel !!!. Bye, Baris |
Last edited by: baris555 at: 09/02/2022 20:01:36 |
|
This contribution was helpful to1 thankful Users |
Follow us on