2/1/2012 4:33 PM | |
Posts: 6 Rating:
|
1LA71662AA61-Z C01 K45 (1LE10011DA434FA4-Z F12 Q02) Our motor details are as follows: 18.5kW, 2930rpm, 3x400V, 50Hz, motor frame-160L, flange type IMB5 (see attachment), with internal heating (230V) and BRAKE(400V). The Siemens replacement looks like 1LA7 166-2AA, which has standard optional brake 2LM8 260-BNA. But the brake has max.operating rpm. (if max.energy utilised) 1500rpm. only. As option, we can order such brake. But we would prefer to order stronger double-disk brake, KFB. Can we get such brake fitted into 1LA7 motor? |
Follow us on