9/2/2017 9:16 AM | |
Posts: 64 Rating: (0) |
Dear All I'm going to use ET200M for 1ms time stamping application as it described in attached manual. I'm wondering if I can use a S7-300 CPU and S7-300 CP for this application. If it's not possible, what is the restriction? is there a special criteria that force me to use just S7-400?! Did anyone has a practical experience with S7300 CPU in conjunction with ET200M for 1ms time stamping application? Sincerely AttachmentET200M_Operating Instruction.pdf (327 Downloads) |
Last edited by: The Helping Hand at: 9/6/2017 8:34:37 AMMerged posts because a lot of duplicates Last edited by: The Helping Hand at: 9/6/2017 8:35:56 AM |
|
9/2/2017 2:16 PM | |
Joined: 1/23/2013 Last visit: 10/17/2024 Posts: 38 Rating: (1) |
I think that 1ms time stamping is supported only in PCS7 with S7-400 and ET200M with certain hardware. BR |
9/2/2017 3:07 PM | |
Posts: 64 Rating: (0) |
In the ET200M manual there are 2 options for time stamping, one," time stamping within the S7 400", and the other, "time stamping outside of S7-400". I attach the respective part of manual related to "time stamping outside of S7-400". It seems it's possible, but I'm looking for a practical experience. Sincerely AttachmentET200M Time Stamping.pdf (340 Downloads) |
Last edited by: mazdak at: 9/2/2017 3:09:29 PM |
|
Follow us on