Industry Online Support
Technical Forum
4/27/2011 3:28 AM | |
Joined: 3/31/2009 Last visit: 7/16/2024 Posts: 191 Rating:
|
hii adtiru, those statement not the parameter for cp525 instead those statement are the statement for sending and receiving data to and from communication partner.. also reset cp525 you should read cp525 first to know how cp525 work.. br rusli
|
7/5/2011 2:01 PM | |
Joined: 2/28/2011 Last visit: 7/3/2024 Posts: 5 Rating:
|
Hi Rusli Saja, Good News. The above thread is getting closed now onwards. Thanks for the input. Thanks to Siemens India - Chennai Team Mr.Senbaga Ganesh & Mr.RajaRam who helped me in the CP 525 com program at S5 PLC. Actually CP525com was programmed "Telegram level". This has been identified by trial & Error type. By reffering the manual COM 525. Chapter 7 section page 49. the above tread is closed. COM 525 Programming Package for the Communication Processors CP 524 and CP525 (S5-DOS) Volume 1/2 regards D.Thiru |
This contribution was helpful to
2 thankful Users |
Follow us on