5/21/2012 11:26 PM | |
Joined: 5/21/2012 Last visit: 7/3/2024 Posts: 24 Rating:
|
Hi I'm trying to come up with a solution for control of a 2 stage HVAC system. I have a packaged AC unit that had two independent refrigeration circuits (ie two compressors two reversing valves) and we are trying to gain more manual control than the installed siemens RWD45 gives us. I have started a logo file which I have attached, this is my first time playing with any form of automation so I may have it all backwards! What I am trying to achieve is the following
The program I have at the moment seems to do what I want except for the intergration of the fresh air damper as I'm still a bit unsure how I should intergrate it (suggestions on this would be great!) Also I think my compressor timing my be a bit crude. Any help or insight would be appreciated, remember i'm a newbee Shaun AttachmentLuxmore Aircon 2.zip (213 Downloads) |
Follow us on