Industry Online Support
Technical Forum
6/21/2014 10:16 AM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (307) |
Hello h2_504 Frankly, this does not make sanse to me too since Sinamics DCM is supplied asa single unit unlike SINAMICS G / S Since Sinamics G / S driveshave seperate CU and Drive Units. and in some cases ( e.g. CU 320 ) one CU can control more than one drive, seperate Telegrams are defined for CU and Drive Units. The Seperate Telegrams for CU and Drives in Sinamics DCM seems to be a hangover from SINAMICS G / S If these is any other rational explaination of this, then I am not aware of the same. Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
Follow us on