3/19/2019 1:22 AM | |
Joined: 9/9/2015 Last visit: 7/16/2024 Posts: 727 Rating: (273) |
Dear changgyun, Try to check the following things: 1. Your user account, do you have Simatic HMI right? 2. The folder that you created for the user project, is there SIMATIC Right? (less likely this issue) 3. Did you try it in a different environment/workstations? |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to1 thankful Users |
4/10/2019 5:55 PM | |
Joined: 9/9/2015 Last visit: 7/16/2024 Posts: 727 Rating: (273) |
Dear changgyun, What you mean is when you use new proj wizard, there is an error during os creation? 1. Have you successfully install the pcs 7? 2. Did you install your pcs 7 with administrator account? 3. Did you add the SIMATIC HMI group in the user that you are log in now? It will be helpful if post a screenshot. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to1 thankful Users |
4/10/2019 6:01 PM | |
Joined: 9/9/2015 Last visit: 7/16/2024 Posts: 727 Rating: (273) |
4. Try insert a cable as well. Make sure your network adapter is okay. May be you could configure a random static ip in it. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to1 thankful Users |
4/25/2019 7:19 AM | |
Joined: 9/9/2015 Last visit: 7/16/2024 Posts: 727 Rating: (273) |
Dear PLC2011, Have you tried all the suggested takes in the above thread? |
Last edited by: JazTai at: 04/25/2019 07:19:40Please give me 5 stars Rating if my post is helpful for you. :) |
|
4/26/2019 7:51 AM | |
Joined: 5/3/2017 Last visit: 5/21/2024 Posts: 673 Rating: (217) |
Hello PLC2011,
that can be the root of the problem. Normaly you install the software "PCS 7 Engineering" and "OS Single Station" on the ES. The Software package "OS Single Station" is need for testing the OS on the ES. Did you know the manual Compendium Part A? In the section Preparation and administration you find all settings you have to do in windows to create an PCS 7 project. With regards |
Follow us on