4/18/2019 9:20 AM | |
Joined: 2/6/2017 Last visit: 2/29/2024 Posts: 11 Rating:
|
hello gentleman's! i have a comunication Profibus DP problem with a Hach Lange controller SC1000. TIA Portal V15.0 the network is attached to this post. PLC is a CPU 1512SP-1 PN and controller have a Profibus Card. GDS files is intalled ,from cd provider,i checked for latest updates is ok. i test the cable ,everything is ok,but i can't reach to the controller. the Profibus interface is 6ES7 545-5DA00-0AB0,with adress 2 Master and the controller with adress 4 Slave. Please help me with an exemple or some advice. Thak you a lot!!!!! Attachmentsc 1000.zip (271 Downloads) |
4/21/2019 12:56 AM | |
Joined: 9/27/2006 Last visit: 7/14/2024 Posts: 12268 Rating:
|
Hello sergiu; The configuration of the Profibus-DP telegram on the SC1000 controller is setup with the controller keypad, as described in the following manual, starting in section 5.12. What telegram structure do you have setup at the moment on the controller? The Profibus modules for data exchange must match the number of bytes used in the SC1000 telegram as it is setup. Hope this helps, Daniel Chartier AttachmentDOC023.52.90007_9ed.pdf (287 Downloads) |
Last edited by: Jen_Moderator at: 4/24/2019 6:34:10 AMAdded PDF as an attachment. |
|
4/22/2019 3:47 PM | |
Joined: 2/6/2017 Last visit: 2/29/2024 Posts: 11 Rating:
|
hello again! If i create a profibus network,then i set for each slave and master adress,should i see a connect status? without setting a telegram or config the slave with actual probes connected! because after i delete and reconfig the controller i see not reacheble? thank you! Attachmentnetwork.zip (266 Downloads) |
Follow us on